Instance Appearance

The announcement banner functionality allows administrators to create and display announcements for the Genix application users. These announcements are displayed as a prominent banner at the top of the application(s), which ensures high visibility and conveys important information to the users quickly.

The information on the announcement banner can include notifications about system updates, maintenance, new features, or any other relevant information that the users need to be aware of.

Users can dismiss the banner if they do not want to read the announcement.